URL:
/es-es/go/akb/201009924/1
Progress bar for C0002 commands (from V8.0 onwards)
Functional description
In the Engineer from V2.12, commands which can be activated…
URL:
/es-es/go/akb/201009928/1
Extension of the torque interface (from V8.0 onwards)
Functional description
The LS_MotorInterface system block has been extended by the…
URL:
/es-es/go/akb/201009930/1
Input for resetting the following error (from V8.0 onwards)
Functional description
At the LS_Feedback system block, the…
URL:
/es-es/go/akb/200909316/1
PROFIsafe via PROFINET
Which products are affected?Safety module SM301 V1.2Function descriptionIn addition to PROFIBUS the safe PROFIsafe…
URL:
/es-es/go/akb/200909317/1
Four safely limited speed values
Which products are affected?Safety module SM301 V1.2Function descriptionIt can now be chosen between four…
URL:
/es-es/go/akb/200909318/1
Safe cascading
Which products are affected?Safety module SM301 V1.2Function descriptionThanks to the 'safe cascading' function several…
URL:
/es-es/go/akb/200909319/1
Response time for the safe speed detection can be set
Which products are affected?Safety module SM301 V1.2Function descriptionThe…
URL:
/es-es/go/akb/201004233/1
EtherCAT communication via AIF with EMF2192IB EtherCAT communication module (from V3.0 onwards)
Function extension:
Besides the CAN…
URL:
/es-es/go/akb/201006029/1
Serial number of the module is displayed in the code and in index I-1018
Function extension:
In order to ensure a clear…
URL:
/es-es/go/akb/201006049/1
Additional device identification for connected CAN devices
Function extension:
If the CAN device is temporarily not available during…
URL:
/es-es/go/akb/201006044/1
New codes L-C1129 for saving the network configuration
Function extension:
By means of the new code L-C1129 (IP address activation,…
URL:
/es-es/go/akb/201006045/1
DHCP (Dynamic Host Configuration Protocol) function
Description
The DHCP function can be activated via the 'Settings' tab in the system…
URL:
/es-es/go/akb/201006038/1
CAN SDO block data transfer
Function extension:
In addition to the standard SDO parameter communication the CAN onboard connection of…
URL:
/es-es/go/akb/201006048/1
Indication of the active network configuration
Function extension:
This display is very useful if instead of a permanently assigned…