URL:
/fr-be/go/akb/20039071/1
Code setting via AIF interface
Question:
Why is there an incorrect value in a code of a Servo PLC or Drive PC, which was set via AIF…
URL:
/fr-be/go/akb/20031787/1
8-Bit divergence with L_ParWrite, date inconsistency
Question:
Why does a code in the PLC which is written with the function…
URL:
/fr-be/go/akb/20031115/1
Download mode for H315 and H410
Question:
Can operating units H315 and H410 change to the download mode without separate function…
URL:
/fr-be/go/akb/20031727/1
Consistent data transmission of position values above task limits
Question:
When angle information for synchro systems are…
URL:
/fr-be/go/akb/20031696/1
Mains supply of 230 V inverters
Question:
How can 230 V inverters be supplied from a three-phase mains (e.g. 3 x 400 V) without N…
URL:
/fr-be/go/akb/20031603/1
What happens after a task overrun?
Question:
What happens after a task overrun?
Answer:
If a task overrun has occurred all…
URL:
/fr-be/go/akb/20031516/1
Two-wire sensor at analog input (as master current)
Question:
How is a passive two-wire sensor connected to the analog input of the…
URL:
/fr-be/go/akb/200400522/1
Receive identifier assigned to two CAN channels within one CAN participant
Question:
What will happen if the same input identifiers…
URL:
/fr-be/go/akb/200400765/1
Simple short commissioning of the Siemens PLC and Lenze profi bus participants
Question: Is there a simple possibility to operate the…
URL:
/fr-be/go/akb/200400541/1
External brake resistor, configuration OC6
Question:
What has to be considered regarding the temperature monitoring when an external…
URL:
/fr-be/go/akb/20031475/1
Linear correction of variables in the HMI project
Question:
How can rounding errors be avoided when entering values because of the…
URL:
/fr-be/go/akb/20031471/1
Oscilloscope function, exporting measured data to Excel
Question:
How can measured data of the oscilloscope function be edited in…
URL:
/fr-be/go/akb/20031470/1
Different task types, task features
Question:
Which task types do Lenze PLCs support?
Answer:
9300 Servo PLC and Drive PLC…
URL:
/fr-be/go/akb/20031410/1
CCTRL touch probe, meaning of the different modes
Question:
In the CCTRL function block four different touch probe modes can be…
URL:
/fr-be/go/akb/20031395/1
Commissioning of system bus adapter EMF2173 IB with Win2000
Question:
The system bus adapter EMF2173IB does not work with WIN 2000?…