URL:
/fr-be/go/akb/20010158/1
Accept positioning profile parameters during positioning
Question:
Do new positioning profile parameters can be accepted or modified…
URL:
/fr-be/go/akb/20010157/1
Increase breakaway torque in case of vector control
Question:
What is the correct reaction like to a too low breakaway torque (e. g.…
URL:
/fr-be/go/akb/20010155/1
Transfer of DDS projects to another PC
Question:
Which files are necessary in order to a make DDS project executable on another PC?…
URL:
/fr-be/go/akb/20010153/1
Absolute encoder for master value selection, selection criteria
Question:
How can a cam drive be adapted to a master value…
URL:
/fr-be/go/akb/20010152/1
Asynchronous motor with feedback system rotates uncontrollably with low speed
Question:
How are uncontrolled revolutions caused…
URL:
/fr-be/go/akb/20010151/1
Arithmetic operations, higher range of values
Question:
How can the range of values applied to arithmetic calculations be extended?…
URL:
/fr-be/go/akb/20010150/1
Arithmetic operation supplies incorrect result
Question:
Why is the result of an arithmetic operation wrong, although it is within…
URL:
/fr-be/go/akb/20010149/1
Inverter is enabled, but shows no reaction to speed set value
Question:
The 9300 drive controller can be enabled (IMP in the display…
URL:
/fr-be/go/akb/20010147/1
Adaption of the motor current in the vector control
Question:
How the can the motor current be adapted manually in the vector…
URL:
/fr-be/go/akb/20010148/1
DC injection brake, response time of the 8200vector, motec
Question:
How long is the response time of the 8200 vector DC injection…
URL:
/fr-be/go/akb/20010146/1
Two poles motor connection, operation at frequency inverter
Question:
Is it possible to connect a two-phase motor to a frequency…
URL:
/fr-be/go/akb/20010145/1
Two pole mains supply of a drive controller with 3 phase mains input
Question:
In what way does the output power drive controller of…
URL:
/fr-be/go/akb/20020399/1
Flying restart circiut - Function of
Application:
Blower Drives with big moment of inertia
Description:
Thanks to the flying…
URL:
/fr-be/go/akb/20010140/1
Sending sync frame from the HMI keypad unit
Question:
How can sync frames be sent with a keypad unit (e.g. H310)?
Answer:…
URL:
/fr-be/go/akb/20010139/1
Saving code settings in a PLC project
Question:
Can the settings of codes be saved in a PLC project?
Answer:
No, this is…