URL:
/fr-be/go/akb/202100055/1
EASY Package Manager: Install only required packages
Function extension:In the EASY Package Manager, the user can limit the amount of…
URL:
/fr-be/go/akb/202000372/1
Change in the 'Options' dialog
Function extension: Category 'CoDeSys 2.3 Converter' has been removedStarting from PLC Designer…
URL:
/fr-be/go/akb/202100043/1
Improvement in the operation of the PLC Designer
Function extension: Extension of Smart Tags with further options for automatic…
URL:
/fr-be/go/akb/202100042/1
Optional inputs of functions
Function extension: Inputs of a function (FUNCTION) for which an initial value has been defined in the…
URL:
/fr-be/go/akb/202100041/1
Multi-selection when activating/deactivating devices
Function extension: Multiple devices can be selected at the same time in the…
URL:
/fr-be/go/akb/202100038/1
New command 'Choose Active Application'
Function extension: The command 'Choose Active Application' is a selection list. This…
URL:
/fr-be/go/akb/202100037/1
New icons in the library manager
Function extension: In the library manager (device tree), the states of the libraries are marked with…
URL:
/fr-be/go/akb/202000365/1
Parameters with many decimal digits
Function extension: Depending on the device series, there are certain parameters whose value is a…
URL:
/fr-be/go/akb/202000363/1
i950 New manual movement type ‚MOL Profile‘
Function extension: i950 from firmware version 1.5 has a new movement type ‚MOL Profile‘.…
URL:
/fr-be/go/akb/202000362/1
Set safe parameters to factory settings
Function extension: On the ‚Safe Parameter List' tab, the safe parameters can be set to their…
URL:
/fr-be/go/akb/202000351/1
Ethernet Tunnel via Profinet Interface
Function extension: The Profinet interface of the controller can be used to log in with the PLC…
URL:
/fr-be/go/akb/202000352/1
EASY Starter supports Lenze controllers c5xx and c750
Function extension: With the EASY Starter from V1.19 onwards, it is possible to…