Create, add or delete a custom device page

Usability is one of the core principles of X4 Remote. This is why X4 Remote allows you to fully customise the pages that you and your users can see in the Portal app. You can add and remove components as you see fit. This way, the users in your company will only see the components that are relevant for them. You can even create your own custom components and manage access to the pages you create for maximal versatility.

When you create a new page, this will be a draft at first. This way you can develop the lay-out of your page thoroughly. When your design is finished, you can publish the draft.

Use the links below for easy navigation.

Create a new page

Please follow the steps described below to create a new page. If you already have a similar page and you only want to make a few adjustments, u can also choose to duplicate an existing page.

  • Go to the Studio, which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
  • Open the main menu, go to Pages, then press[add new page] in the bottom right corner.
  • Fill in in the desired name (identifier for the studio) and title (identifier for the portal), then press [add].
  • Click on the name of the page, add components and customise the page appearance. All actions will be saved in a draft version of the page automatically.
  • When you are happy with your configuration, Publish the page with one click on the button.
  • Confirm by clicking on [Publish page].

Unhappy with your draft?You can choose to remove your draft by pressing [revert to published version] in the options menu on the right of the publish button.

Add a page to a device

Add a page to multiple devicesYou can add a page to multiple devices, but you need to make sure that the identifier of the data sources is the same for all the devices you want to add that page to.

To make a page visible for your users, you have to add the page to the devices you want to use the page for. Please follow the steps described below to add a page to a device.

  • Go to the Fleet Manager which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
  • Open the main menu, go to devices, select the device you would like to link a page to.
  • Go to View, then click on [add a page].
  • Select the desired page title and select the desired access category, then press [add].

Edit or remove a page from a deviceIn the same menu as where you add a page to a device. You can also very easily [re-arrange] or [remove] a page.

Make changes to a page

Change page appearanceYou can always add or remove components and make other changes to the appearance of a page.

After you published your own page, you can always make changes to the settings of the page and. remove the page if you no longer have any uses for it. Please follow the steps described below to make changes to a page.

  • Go to the Studio which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
  • Open the main menu, go to Pages, then press [more] on the right side of the overview page. You now have five options:
    1. You can choose to remove your draft by pressing [revert to published version].
    2. You can [Duplicate] the page to use it for different machines with small differences in configuration.
    3. Choose [Rename] to change the page name. Fill in the new name and press [confirm].
    4. Choose [Set as default] to make this page the default page that will be added to a new device.
    5. Choose [Remove] to delete a dashboard. Confirm by clicking on [Remove page].
Kontaktformular