OPC-UA

Supported hardware and firmware

Cloud Notify via OPC-UA is supported on the x500 in firmware 3.7 and up. Please upgrade your firmware if you are running an older version.

Activate Cloud Notify

Please first activate Cloud Notify (or start the 30 day free trial) if you haven't already.

The Second step in Cloud Notify is setting up a data source. This is done by selecting a communication protocol and defining the variables. This article shows you how to do this for communication via OPC-UA.

  • PLC setting
  • Select a communication protocol
  • Add variables
  • Test variables
  • Manage variables

PLC setting

On some PLCs you may have a (sign &) encrypt setting. You will need to turn off this encryption setting so the x500 can communicate with your device. Don’t worry, communication between the x500 and X4 Cloud is always secure (more info).

Select a communication protocol

You first have to select a communication protocol. This is the protocol that the x500 will use to communicate with the PLC.

  • Go to the Fleet Manager app, which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
  • Open the Main menu, go to Devices, and select the concerning device.
  • Click on the Add a service icon in the left menu, select [Data source], and then select [OPC Unified Architecture].
  • Enter the requested information (details below) and click on [Add].
Field Description
Name Enter a name for the data source.
Identifier The identifier ensures that every data source remains unique, even if they share the same name.
IP address

Enter the IP address of your PLC.

Port The port number will be entered automatically (Port 4840 for OPC-UA).
Authentication Select the OPC-UA server’s authentication type and enter your credentials if required.
Polling sleep time

To log data as accurately as possible, the x500 continuously asks the variables’ values from the PLC (this does not count towards your license’s dps/hr). While the x500 does wait for the PLC to reply before asking again, in very rare cases this may noticeably impact the PLC’s performance.

In such a rare situation you may want to change this setting to 100ms or higher. In general “None” is recommended for Cloud Logging to be as accurately as possible.

Add variables

Once you’ve added a data source and selected a communication protocol, you can start adding variables. You can do this by following the steps below:

  • Expand the Data source service and go to [Variables].

You’ll need to know your variable’s data type and address. Below you’ll find a table containing all available data types and their equivalents in X4 Remote.

Offline (PLC) Online (X4 Remote)
Boolean Boolean
SByte Int8
Int16 Int16
Int32 Int32
Int64 Int64
Byte UInt8
UInt16 UInt16
UInt32 UInt32
UInt64 UInt64
Float Float32
Double Float64
String String

The variable’s address consists of a namespace index and identifier. In the example below we’ll be using UaExpert to find these attributes.

  • Open UaExpert, press [Server] and then [Add].

  • Select [Advanced], enter the IP address and port number (default 4840), separated by a colon, and press [OK].

  • If you’re not already automatically connected, you can manually connect to the added server by going to [Server] > [Connect].
  • Once you’re connected, find and select your variable in the “address space“-window in the bottom left.
  • You should see the variable’s NamespaceIndex and Identifier in the “attribute“-window in the top right.

Now you have all the necessary information to add the variable to your data source and can now choose to:

  • Manually add new variables
  • Import variables from a file (or device)

Tip!

It is advisable to add variables in small batches and test them to verify their configuration.

Manually add new variables

  • Go back to where you were in X4 Remote.
  • Click on [Add variable] in the bottom right corner.
  • Enter the requested information (details below) and click on [Add].
Field Description
Name Enter a name for the variable.
Identifier The identifier ensures that every variable remains unique, even if they share the same name.
Type Select the variable’s data type (bool, int, float, etc).
Length (for String data types only) The String length.
Namespace Enter the namespace index.
Identifier type Select the identifier type.
Value Enter the identifier value.
Factor Multiplies the value (leave empty if the data type is boolean).
Unit Displayed text behind the value.

Temporary disconnect

After this next step, the config push, the device may temporarily disconnect and LAN communication may be temporarily interrupted while it's applying the new settings. This may take a minute.

You have now made the changes in X4 Remote, but these are not yet active in your device. You will need to push your changes to your device for them to take effect.

  • Click [Push config to device] in the top right corner.

Next step

Now that you've added the variables, you can test if they're configured properly.

Import variables from a file (or device)

You can easily and effortlessly copy variables from one device to another by exporting the concerning variables (view the “Manage variables” part of this article) and then importing them in your new device. Alternatively, you can manually prepare your variables in the required CSV format to load them all at once into your configurator. The CSV file structure is explained in our Import variables article.

  • Click on [Import from CSV-file] in the top right corner of the screen.
  • Select a CSV file to import and click on [Open].

Temporary disconnect

After this next step, the config push, the device may temporarily disconnect and LAN communication may be temporarily interrupted while it's applying the new settings. This may take a minute.

You have now made the changes in X4 Remote, but these are not yet active in your device. You will need to push your changes to your device for them to take effect.

  • Click [Push config to device] in the top right corner.

Next step

Now that you've added the variables, you can test if they're configured properly.

Test variables

The test utility is used to check if all the added variables are set correctly. It shows the communication status with the PLC and displays each variable’s current value if everything is configured correctly. If not, the values will stay empty. The test utility will attempt to update values every 0.5 seconds, regardless of how often it’s actually being logged (this does not count towards your license’s dps/hr). Please follow the steps below to test your variables.

  • Expand the Data source service, go to [Variables], and click on [Run test] at the top.

A connection will now be set up to stream the data directly to your computer, using:

Port Transport protocol Application protocol
443 TCP WebSocket

You will see live values of all variables, if the configuration is set up correctly.

Unexpected result?

If the test utility shows unexpected values, please check if the addresses and data types of all variables are entered correctly. If you get an error message, please check Common error messages for more info. If you get no data at all, please also check that the above listed port and protocols are not being blocked by your computer's or company's firewall.

Next step

Now that you've tested the variables, you can view our "Configure data tags" guide to start logging.

Manage variables

You can view all defined variables on the variables page:

  • Expand the Data source service and go to [Variables].

You can [Edit] individual variables, [Remove] individual or a selection of variables, and export all or a selection of variables.

Variables can be selected by clicking the checkbox on the left, or you can select them all by clicking the checkbox at the top.

 

Kontaktformular