Audit Log

The audit log contains a detailed event log for all changes that have been made within the X4 Remote company. The audit log or audit trail can be used to see what has changed within the company. In the audit trail you can also see which person, server or device triggered a certain change, and when the change occurred.

This is an Alert

You need to have a role with audit trail viewing rights to access the audit trail in your company.

Some of the fields in the audit trail are displayed as JSON code. Therefore, some knowledge on this topic might be necessary to understand certain details.

Please follow the steps described below to view details about a certain event.

  • Go to the Admin which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
  • Open the main menu, go to Audit trail, then click on [Details] for the event you would like to see in detail.
  • Please look at the table below for a list of fields displayed in the event details section.
Field Description
Date and Time The date and time when the event occurred in the configured timezone.
Timestamp (UTC) The UTC timestamp of the date and time.
Action The kind of action that occurred with the event (e.g. CREATE, UPDATE and DELETE)
Target The object to which the action applies (e.g. a router or user)
Actor The person, server or device that caused the event.
Topic Detailed information about the target and the of which a target is part.
Before The configuration as it was before the event occurred
After The configuration as it was after the event occurred

Time limit
Events in the audit trail will be saved for a period of 6 months. This means that you can review past events up to a maximum of 6 months.

Kontaktformular