URL:
/es-es/go/akb/202400254/1
Trend system
Function-extension:With the trend system, variable values can be recorded in a trend and their current or historical…
URL:
/es-es/go/akb/202400259/1
DesignTime: Cross-reference in the server is not available after project update
Corrected from:EASY UI Designer V1.6Behavior of the…
URL:
/es-es/go/akb/202400257/1
DesignTime: Startup files are not updated when the project is updated
Corrected from:Behavior of the new version:Description of…
URL:
/es-es/go/akb/202400238/1
DesignTime - Pages/Views: When adding existing pages to the project, they are overwritten without warning
Corrected from:Behavior of…
URL:
/es-es/go/akb/202400256/1
DesignTime - Style: Properties window does not contain all properties in the styling view
Corrected from:EASY UI Designer V1.6Behavior…
URL:
/es-es/go/akb/202400240/1
AlarmLine - Line break can be configured for alarm information in the alarm line
Function Extension:From version 1.6 it is possible to…
URL:
/es-es/go/akb/202400255/1
DesignTime: Submenu height does not expand dynamically
Corrected from:EASY UI Designer V1.6Behavior of the new version:Any number…
URL:
/es-es/go/akb/202300210/1
Design Time - Controls - Bar: Property Limits (Collection) not functional
Corrected from:EASY UI Designer V1.5Response of the new…
URL:
/es-es/go/akb/202400241/1
Runtime - Trend: If the configuration is invalid, no comprehensible error messages are displayed in the browser
Lifted from:Behavior…
URL:
/es-es/go/akb/202300525/1
Design Time: EASY UI Designer crashes when a control is added after editing the current style of the CheckboxGroup control
Corrected…
URL:
/es-es/go/akb/202300515/1
Design Time: The EASY UI Designer will be closed with an exception when the connected controller is restarted via "0x2022:035" in PLC…
URL:
/es-es/go/akb/202300519/1
FAST UI Runtime - Historical Alarms: Status "InactiveAck" is not displayed.
Corrected from:EASY UI Designer V1.5c5x0 FW V1.11Behavior…